Technical FAQs

Ask a Question

Do the LAD9 & LA9D 4-pole power connection kits consist of a set of two connections?

Issue: 
Do the LAD9 and LA9D 4 pole kits includes both line and load connections? 

Product Line:
Tesys D line accessories

Environment:
Products sold and used in the United States
 
Cause:
 Identifying kit components
 
Resolution:
 
No, only the load side connectors are included.


CTA-ID : 2014459
Was this helpful?
What can we do to improve the information ?