Technical FAQs

Ask a Question

Need info on a GADD MKII(2) ground relay indicator<br />

See Schneider Canada, There are 2 versions, 120V control is a CADD2-1, & a 240V control is a CADD2-2. Avail thru Caravelle location, (Waterman factory location) Also on Schneider Canada web site

CTA-ID : 2014207
Was this helpful?
What can we do to improve the information ?