Technical FAQs

Ask a Question

Are the replacement heads for an XCKML switch the same as those used on the XCKL?

Yes and no, Yes the XCKML uses the same heads and levers as the XCKL however the heads and bodies on the XCKML can not be replaced in the field The XCKML must be ordered from the factory as a complete unit so that the head and body can be tested together.

CTA-ID : 2014205
Was this helpful?
What can we do to improve the information ?