Technical FAQs

Ask a Question

What are the 7400ENT(_) Fingersafe Terminal Block Cover Kits for Epoxy Resin Encapsulated Transformers?

Fingersafe Terminal Block kits

Product Line:
LV Transformers

Applies to LV transformers by SquareD/Schneider Electric

Epoxy Resin Encapsulated Transformers have optional terminal block cover kits available


It is a terminal block and enclosure extension (adds 1.5`` or 2`` height to the installation, see the Digest). The customer would wire to a terminal block, instead of with wire nuts, thus providing a fingersafe connection.

CTA-ID : 2014203
Was this helpful?
What can we do to improve the information ?