Technical FAQs

Ask a Question

What would be the part number of the pilot relay for the shorting contactor for the ATS48 soft starter?

There are two basic requirements.
1 - Pilot relays must have a coil burden 414 VA or less. (1.8A for 230VAC)
2 - The relay contacts must be rated to handle the coil of the shorting contactor.


CTA-ID : 2014192
Was this helpful?
What can we do to improve the information ?