Technical FAQs

Ask a Question

Can I get a STOP push button for an 8539 NEMA 7/9 combination starter?

Issue:
Can I get a STOP push button for an 8539 NEMA 7/9 combination starter?

Product Line:
Nema combination starters sold and supported in the USA.

Environment:
Maintenance

Cause: 
Selection

Resolution:
Yes. The part number is 2949520605 for the stocked red STOP button. You must also use a 9001KA1 contact block for that three position switch.

Revision:  Effective 2011, Nema 7 and 9 enclosures are no longer available for our Nema contactors/starters.  The 2949520605 is available strictly for replacement purposes.  

CTA-ID : 2014443
Was this helpful?
What can we do to improve the information ?