Technical FAQs

Ask a Question

XSAV11801 is it rated for a Nema 7 & 9 application.

XSAV11801 is rated for Nema 3,4,6,12, and 13 applications. Our solid state sensors, except for NAMUR, are not rated for hazardous applications. NAMUR may only be used in hazardous applications when used with an intrinsically safe barrier system .

CTA-ID : 2014668
Was this helpful?
What can we do to improve the information ?