Technical FAQs

Ask a Question

Why does the drive macro say customized even after setting the macro to VT Variable Torque, Hdg Material Handling or GEn General use with the ATV58 drive?

The drive is not loosing its memory.
As the manual states: If you customize the I/O to your application, the macro-configuration screen displays CUS:Customize.

Anytime changes are made to the parameters after initially set macro, it is no longer at its factory defaults and then becomes a customized version of the macro you programed into it which is why you see the change. There is no need to set the macro again if the macro configuration displays customized.


CTA-ID : 2014584
Was this helpful?
What can we do to improve the information ?