Technical FAQs

Ask a Question

What is the rated transient output current for the Altivar 58 drive at Constant Torque rating?

160% of nominal NEC rated motor current for 60 seconds.

This does not apply to ATV58 drives from ATV58HC10N4 and larger, as these drive are not rated for CT applications.

CTA-ID : 2014532
Was this helpful?
What can we do to improve the information ?