Technical FAQs

Ask a Question

How many auxiliary contacts can be installed on a NEMA size 0, 1, or 2 two-speed starter?

Qty (4) are allowed for each starter; however, they must all be installed on the outer side of the starter, as the mechanical interlock between the starters prevents any auxiliary contacts from being installed on the inner side.

CTA-ID : 2014178
Was this helpful?
What can we do to improve the information ?