Technical FAQs

Ask a Question

What is the number and size of the blank legend plate for the K115 cam switch?

Legend plate number is KZN103. It is 88 m X 88 mm front plate mount used with 115 and 150 Amp.


CTA-ID : 2014174
Was this helpful?
What can we do to improve the information ?