Technical FAQs

Ask a Question

Do all the 8839 Econoflex NEMA 3R Enclosed drives have a hood over the top?

No, only the 30-100hp at 460V and the 15-50hp at 208/230V would have a hood over the top.
There are no hoods on the smaller NEMA 3R econoflex drives.


CTA-ID : 2014168
Was this helpful?
What can we do to improve the information ?