Technical FAQs

Ask a Question

What is the part number for the touch up paint for the Econo-Flex?

It is Grey and the part # is PK49SP.

The same paint is used on the Econo Flex, the Marley package and the 18-pulse drive.


CTA-ID : 2010138
Was this helpful?
What can we do to improve the information ?