Technical FAQs

Ask a Question

Do we have a 48 vAC coil for the 8501 CO6 relay?

See voltage codes in the GIC Help File showing the V17 is the 48 v AC coil code for the 8501 C type relay.

CTA-ID : 2013926
Was this helpful?
What can we do to improve the information ?