Technical FAQs

Ask a Question

How can the Output Phase Fault (OPF) for the ATV58 be disabled?

Keep in mind that this will disable the output phase loss protection. It may be advisable to provide external phase loss protection for the motor by using overloads with single phase sensitivity.
With the keypad unlocked, go into menu #6 (FLt fault menu).
Scroll to the Output Phase Loss (OPL) parameter.
Press ENT (enter).
Scroll to NO.
Press ENT (enter).
Cycle power, allowing the display to go blank before restoring power.
Return the display to the desired screen and locked condition.

CTA-ID : 2014354
Was this helpful?
What can we do to improve the information ?