Technical FAQs

Ask a Question

What is the catalog number for the center pole with flash cover on an H366 Series D2?

40512-140-50 switch base and 40512-057-50 arc suppressor is obsolete and no longer available.


CTA-ID : 2014413
Was this helpful?
What can we do to improve the information ?