Technical FAQs

Ask a Question

Can a 9012GFWM4 be factory set at a certain pressure level?

Yes, if requested when ordering. Add form Y1 and specify setpoint. Set points must lie within the range of the switch, and must define the high and low pressures.

CTA-ID : 2014406
Was this helpful?
What can we do to improve the information ?