Technical FAQs

Ask a Question

What are the dimensions and the weight on the ATV58HD23N4XZU?

Width = 9.06 in (230 mm)
Height = 16.35in (415 mm)
Depth = 8.27 in (210 mm)
The weight is 31 lb (13.9 kg)


CTA-ID : 2013922
Was this helpful?
What can we do to improve the information ?