Technical FAQs

Ask a Question

Customer asks if the Minibreak Compact Height Switch can be used to daisy chain several switches?

Customer was advised that the standard product does provide a two barrel lug on the line side of each switch which can be used for this purpose.

CTA-ID : 2014400
Was this helpful?
What can we do to improve the information ?