Technical FAQs

Ask a Question

What is the part number for the motor protecting output filter for the ATV58HD79N4XZU?

Selection of output filter is based on motor amps and HP.
If this is for a 75 HP motor, use the KLCUL110A2. It is rated for 110 amps.
If this is for a 100 HP motor, use the KLCUL130A2. It is rated for 130 amps.


CTA-ID : 2014399
Was this helpful?
What can we do to improve the information ?