Technical FAQs

Ask a Question

Can the PQ4220G be installed on vertically mounted busway?

The PS4220G plug-in unit is recommended to be used on vertically mounted busway. However, if the PQ4220G must be used, an additional support system must be provided by the installer.

CTA-ID : 2014397
Was this helpful?
What can we do to improve the information ?