Technical FAQs

Ask a Question

Can an H363DSWC be made from components in order to expedite delivery?

No, the switch construction is too complex to attemp building in the field. The UL listing would be void if attemped. The best suggestion would be to place the order and expedite through channels.


CTA-ID : 2014645
Was this helpful?
What can we do to improve the information ?