Technical FAQs

Ask a Question

What is the solid neutral for HCP54868SU?

HCPSU8SN
or
HCPSU8SNCT which includes a neutral CT


Terminations are as follows:
Main Lugs
(8) #3/0 - 750MCM
Branch
(34) #4 - 14
(9) #14 - 1/0
(7) #6 - 350MCM

Revised 4/27/04



CTA-ID : 2014363
Was this helpful?
What can we do to improve the information ?