Technical FAQs

Ask a Question

Does the ATV28 have brake logic programming function to operate external mechanical brake like the ATV16 that had the general purpose option card installed?

No.

To get brake logic programming would need to replace the ATV16 with an ATV58 unit.


CTA-ID : 2014361
Was this helpful?
What can we do to improve the information ?