Technical FAQs

Ask a Question

What are the components of the 9999SA13 push button kit?

Qty 2 - 9001 KA1 - Contact blocks.
Qty 1 - 9001 KN201BP - ``START`` legend plate.
Qty 1 - 9001 KN202RP - ``STOP`` legend plate.
Qty 1 - 9001 KN203BP - ``ON`` legend plate.
Qty 1 - 9001 KN204RP - ``OFF`` legend plate.
Qty 1 - 9001 SKR1B - Black push button operator.
Qty 1 - 9001 SKR1R - Red push button operator.

Note - The 9999SA13 also includes a pre-cut wiring harness which is not available as separate item, customer will be required to provide necessary wiring.


CTA-ID : 2014355
Was this helpful?
What can we do to improve the information ?