Technical FAQs

Ask a Question

What is the recommended fuse type for a GK1DF?

Product Line:
GK1 Fuse Holder

Our recommendation for fuses are: cartridge fuse type , 32 amp and size of cartridge fuse or link 0.4 x 1.5 inches (10 x 38 mm)
Possible references.

Type CC

Type aM catalog number 9080CT0001

Type gL/gG catalog number 9080CT0001

CTA-ID : 2014117
Was this helpful?
What can we do to improve the information ?