Technical FAQs

Ask a Question

How do I obtain a Certificate of Conformity or Compliance?

Certificate of Compliance is a form letter that says we made the product in accordance with the standards that we label it with. Normally no charge.

A Certificate of Conformance tests the product as it is being assembled, according to the testing or standard required by the customer. The results are documented and supplied as a certificate to the customer with the device. There is a charge for this service based on testing required. The customer must supply us with the list of requirements before we can quote a price. In addition, this certificate must be ordered at the time of original purchase because testing must be done while the device is being assembled and certified.

The CE mark, declaration of conformity, is available on the internet.

CTA-ID : 2014619
Was this helpful?
What can we do to improve the information ?