Technical FAQs

Ask a Question

QMB30R - How many QMB switches or busway plug in units will this kit convert for use with Class R fuses?

Product Features

Product Line:
QMB Accessory

Clarifiying number of kits needed

The QMB30R provides six (6) Class R fuse clips that will convert two (2) QMB switches or busway plug in units to accept Class R fuses only. 
NOTE: Most QMB branch switches are provided as twin units, containing two (2) switches. One QMB30R will convert both of the switches provided in the twin unit. 

CTA-ID : 2014335
Was this helpful?
What can we do to improve the information ?