Technical FAQs

Ask a Question

Are fusible plug-in units 100% rated?

Yes they are 100% rated. They can safely carry the nameplate current. HOWEVER, UL and NEMA only allow fuses up to 80% of the nameplate rating to be installed in these plug-in units.


CTA-ID : 2014320
Was this helpful?
What can we do to improve the information ?