Technical FAQs

Ask a Question

What is a GF1200I ground slave module?

The GS1200I is used as a collection point for grounds in a large area such as an intesive care or coronary care ward . It is used when the equipment ground bus is not conviently located or cannot accept a large number of ground connections.
Also refered to as a master ground module

CTA-ID : 2014080
Was this helpful?
What can we do to improve the information ?