Technical FAQs

Ask a Question

What is the enclosure material of the Class 2510 Type FW* and Type KW* manual device?

Die cast Zamak (Zinc Die Cast); zinc based alloy containing magnesium, aluminum and copper.


CTA-ID : 2013844
Was this helpful?
What can we do to improve the information ?