Technical FAQs

Ask a Question

Does the EDB breaker used in the NF panel have series ratings?

Yes . Refer to the front of the panelboard section of the current Digest

This information is also listed in the information manual shipped with the panel.





CTA-ID : 2014588
Was this helpful?
What can we do to improve the information ?