Technical FAQs

Ask a Question

If customer has an 800 amp M frame breaker in an I Line panelboard, can they take off the undervoltage trip and use the breaker without the undervoltage trip?

Issue:
If customer has an 800 amp M frame breaker in an I Line panelboard, can they take off the undervoltage trip and use the breaker without the undervoltage trip?

Product Line:
Circuit breakes.

Environment:
Products sold in the United States.

Cause:
Product features.

Resolution:
The undervoltage trip on the M frame breaker is field installable so he can take it off and use the breaker without it.


CTA-ID : 2014583
Was this helpful?
What can we do to improve the information ?