Technical FAQs

Ask a Question

Customer asks if the HPAFK can be attached with #4 screws in lieu of rivets?

No. Per OSHA it is important that the attachment not be removeable without use of special tools or unreasonable force. It needs to be ``tamper evident`` and screws would not be.
Customer was advised that we would not recommend using anything but the drive-screw that is provided. Lock-tight may be used if deemed necessary.

CTA-ID : 2014576
Was this helpful?
What can we do to improve the information ?