Technical FAQs

Ask a Question

Customer asks if the medium voltage dry type pad mount transformers are provided with a ul listing?

As of 4/3/06 the kva range of 112.5 through 5000 kva can be UL listed.


CTA-ID : 2014575
Was this helpful?
What can we do to improve the information ?