Technical FAQs

Ask a Question

Customer has a HU361RB and needs to know if it will accept two wires per phase and neutral?

Yes, as standard it will accept (1) #13-6 Al or #14-6 Cu OR
(2) #14-10 CU only Solid or Stranded.


CTA-ID : 2014546
Was this helpful?
What can we do to improve the information ?