Technical FAQs

Ask a Question

What are the repair parts for the H361-2RB Series F5? (maybe shown as F05)<br />

The repair parts for the H361-2RB, series F5 (F05) are as follows. No other parts are available.

Line Base Assembly -40566-039-50 (requires one per switch. Arc suppressor assembly not included)
Load Base Assembly - 4056604150 (requires one per switch)
Arc Suppressor Assembly - 40566-355-50 (requires one per switch)
Lug Assembly - 40251-016-52 (per lug)
Switch Mechanism - 40566-469-50
Handle Assembly - 40566-635-50
Handle Gasket - 40566-031-01
Lockplate - 40566-721-01



CTA-ID : 2014280
Was this helpful?
What can we do to improve the information ?