Technical FAQs

Ask a Question

Does Square D offer a 400 Amp, 600V AC, NEMA 4X, Stainless Steel, Double Throw Safety Switch?

Product Availability

Product Line: 
Double Throw Safety Switches

Maximum amerage switch


YES, the catalog number is 82345DS. This catalog number is a Non-Fusible, 3-Pole, 600V AC - 250V DC MAX., 400 Amp MAX. in a NEMA 4-4X-5, 304 Stainless Steel Enclosure. The Solid Neutral Assembly that can be used with this switch is catalog number DT400N. SEE DIGEST AND CAD DRAWING FOR ALL SPECIFICATIONS BEFORE OBTAINING.

CTA-ID : 2014274
Was this helpful?
What can we do to improve the information ?