Technical FAQs

Ask a Question

What is the continuous output current rating for the ATV58HD46M2XZU drive with single phase 208/230V for ?

This depends on the application and settings:
For Constant Torque applications the rating is 116 amps with switching frequency set for 2 kHz or less.
For Constant Torque Low Noise and Variable Torque applications the rating is 88 amps with switching fequency set for 4 kHz or greater.


CTA-ID : 2014533
Was this helpful?
What can we do to improve the information ?