Technical FAQs

Ask a Question

On the 9025GXW family of temperature switches what is the maximum allowable temperature ?

Depending on which one you pick, it varies between 190 and 450 degree F. Refer to page 20-17 of the 173 digest for specify part numbers and ranges.


CTA-ID : 2014526
Was this helpful?
What can we do to improve the information ?