Technical FAQs

Ask a Question

How many 9001KA contact blocks can be mounted on 9001KS or 9001SKS spring return selector switch?

Two (2) blocks mounted side by side only for any 2, 3 or 4 position spring return selector switch (non-illuminated, illuminated or keyed).


CTA-ID : 2014271
Was this helpful?
What can we do to improve the information ?