Technical FAQs

Ask a Question

What wire size will the EDB lugs accept?

The EDB EGB EJB (15 - 30 A) breakers will accept:
#12 - #6 AWG Al or
#14 - #6 AWG Cu

The EDB EGB EJB (35 - 125 A) breakers will accept:
#12 - #2/0 AWG Al or
#14 - #2/0 AWG Cu


CTA-ID : 2014262
Was this helpful?
What can we do to improve the information ?