Technical FAQs

Ask a Question

What is the part # for the manual speed pot that is used on the 8804 PT drive with the P10 Option?

The part number is 52011-367-50. However,the  manual speed pot assembly is obsolete .


CTA-ID : 2014516
Was this helpful?
What can we do to improve the information ?