Technical FAQs

Ask a Question

What is the hp and amp rating of ATS46C14N unit?

It is good for 100hp @ 460V for Standard Duty and 75hp @ 460V for Heavy Duty application. The amp rating is 145 A.


CTA-ID : 2014250
Was this helpful?
What can we do to improve the information ?