Technical FAQs

Ask a Question

How many field installable electrical accessories can be added to an MA or MH breaker?

2 accessories can be field installed, 1 in each port. If a bell alarm is installed (factory only), only one accessory can be field installed. A bell alarm and two other accessories can be factory installed.


CTA-ID : 2014499
Was this helpful?
What can we do to improve the information ?