Technical FAQs

Ask a Question

Customer has a Nema 3R load center and wants to know if they can take out the interior and put it into a Nema 1 box?

NO, must use only the same interior that comes with each type of load center.


CTA-ID : 2014491
Was this helpful?
What can we do to improve the information ?