Technical FAQs

Ask a Question

Customer supplied the A200L hub for the SC3040M200F and it doesn`t work.

Customer needs to make sure that the adapter plate AAP is used with the hub as the A200L is a A hub and needs to have the adapter for mounting to the SC3040M200F.


CTA-ID : 2014227
Was this helpful?
What can we do to improve the information ?