Technical FAQs

Ask a Question

Can a KAB36150 be replaced by a KA36150?

Yes they can be installed in same panel. The only difference is that the KAB36150 has screws to clamp the jaws to the bus.

CTA-ID : 2014716
Was this helpful?
What can we do to improve the information ?