Technical FAQs

Ask a Question

What are the dimensions and the weight on the ATS48D17Y, ATS48D22Y, ATS48D32Y, ATS48D38 or ATS48D47Y soft starter?

The entire width of the unit is a = 6.30 in (160 mm), the entire height of unit is b = 10.83 in (275 mm), the entire depth of the unit is c = 7.48 in (190 mm), and the weight is 10.8 lb (4.9 kg).

See the associated literature for additional details regarding mounting of this soft starter unit.

CTA-ID : 2014474
Was this helpful?
What can we do to improve the information ?