Technical FAQs

Ask a Question

Do the 8911 Definite Purpose starters have a selectable automatic or manual reset switch on the overload relay?

Issue:
Do the 8911 Definite Purpose starters have a selectable automatic or manual reset switch on the overload relay?

Product Line:
Definite Purpose Starters

Environment:
Products sold and used in the United States

Cause:
automatic reset required

Resolution:
At one time, Square D offered an 8911 definite purpose starter with a bimetallic overload relay. These units were selectable from manual to automatic. Today`s 8911 is offered only with melting alloy overload relays which cannot be converted from manual to automatic reset.


CTA-ID : 2013121
Was this helpful?
What can we do to improve the information ?